LAVA 2020.09
  • Index
  • Contents
  • Site
      • Introduction to LAVA
      • Contents
      • Glossary of terms
      • Getting support
  • Page
      • Advanced Use Cases
  • « Debugging LAV...
  • Writing jobs ... »

Advanced Use CasesΒΆ

This section seeks to provide help for several aspects of working with the Lava Dispatcher Design from the perspective of lab admins and LAVA users. The developer documentation will continue to evolve and feed into this section over time.

  • Writing jobs using Secondary Connections
    • Secure Shell connections (ssh)
      • Delaying the start of a job using Multinode
      • Picking up the data in the guest role
      • Test definition for the host role
      • Test definition for the guest role
      • Complete Multinode test definition
  • Replacing VMGroups using Secondary Connections
    • Structure of an example job for a mustang
      • Notes
    • Running operations inside the guest VM

Back to top

© Copyright 2010-2020, Linaro Limited.
Created using Sphinx 1.8.4.